Other Parts Discussed in Thread: INA226, PGA281
Hello
I'm using current sense amplifier to detect the speaker failure in my project. I have chosen INA190 as current sense amplifier wherein my design constraints are
Vvs =3.3V , Vcm = 12V , Imin = 1uA , Imax =2A(4W speaker with 3 ohm impedance gives 1.333A) , Gain = 500V/V , Vref =0 , Current in sleep mode less than 1uA.
1) Whether INA190 is suitable for all my design constraints?
2) What is the maximum current Imax that I can consider which is supported by INA190.
3) Whether error of 0.3% is acceptable if the output of this is to drive an ADC.
Please help me out in this concern.
Regards
Nidhi P Shetty