Hello. Reading the LMP8358 datasheet, I can't figure how to connect this op amp in a circuit to amplify voltage. I have my doubts relate to pins FB, REFF and REFS. Can anybody explain me their functions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. Reading the LMP8358 datasheet, I can't figure how to connect this op amp in a circuit to amplify voltage. I have my doubts relate to pins FB, REFF and REFS. Can anybody explain me their functions?
Very simple, as follows. At photodiode, I have a pulsed signal (AC).
What I want is a lowest DC offset possivel at output. I want Vout=0V for Vin=0V. How to I get that using Refs pins? I'm also very interested in linearity.
I'm actually using the ADA4350ARZ from Analog. Can you compare this chip with yours? Can you convince me that I should use yours istead, for other reasons besides the price?
Please, feel free to write me to my email <ricardo.moreira(at)techchrom.com.br>. Send me some connection circuits if you like.
Based on your given information ADA4350 is the better choice. If you want 0V to 5V out you will need to use id with asymmetrical supplies like +6V, -5V. You need to look at output swing characteristics. ADA4350 is better suited for photodiode application since you can use large external feedback resitors and external compensation.