This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ACF2101 Switched Integrator

Other Parts Discussed in Thread: ACF2101

Hi All:

I am working with a design that uses the IVC102 but I need to add a null offset to the input to zero the detector offset out.  The IVC102 does not have an input that I can use on that chip but the ACF2101 show that it has both the + and - input available on the chip but can use it?  I noticed that the + input on the block diagram connects to the Sw Com.  I have 7 individual detector channels that I want to connect to the ACF2101 individually but I want to adjust the offset for all of them with the same offset circuit.  Does anyone know if you can use the plus input and leave the Sw Com open?