Part Number: INA180
Other Parts Discussed in Thread: INA190
Hello,
We want to measure current on signal line with INA180 EVM and DMM 6 ½ digit following requirements as below:
“24mA with a minimum resolution of 1uA and accuracy of 25 ppm reading + 5 ppm full scale”.
Theoretically we can prove that it is possible to do it following respectively datasheet of INA 180 and DMM but we have some questions as regard of Aging/Endurance test results, proving INA 180 solution meets accuracy over time. Do you have some data on that?
Rsense resistance choisen is VCS 1610Z With ultra-low TCR±0.2ppm/°C with Resistance Value 1Ω
We will maintain the work floor temperature between 22C to 28C.
How can I provide a certified uncertainty analysis (approved by 3rd party ISO 17025 accredited laboratory or other) of the entire system (resistor / amplifier / volt meter)?
Best regard
Alain Lopez