Other Parts Discussed in Thread: TINA-TI, , ISO224, AMC1300, AMC1302
Tool/software: TINA-TI or Spice Models
The Input of AMC1211-Q1 is on module 1. The output of AMC1211-Q1 is on module 2. If Vdd1 is lost while Vdd2 is powered, what is the differential output level? I want the output to be zero. Currently I use ACPL-C78A. The output is 5V when Vdd1 is lost, which causes a lot of problems. I hope TI does not have this drawback.
Sam