Part Number: OPA207
Hello,
The OPA207 datasheet describes that it can replace from OP-177.
Certainly, the electrical characteristics has the same or higher performance,
however, I have one concern.
In ADI OP177 datasheet, it is written that as below.
The OP177’s combination of outstanding specifications
insure accurate performance in high closed-loop gain applications.
On the other hand, in TI OPA207 datasheet we can see as below.
OPA207 is stable in unity gain and provide excellent
dynamic behavior over a wide range of load
conditions.
I'm going to try to replace from OP177 to OPA207 in a load cell application, the gain is about 100.
Is it not recommended ? Or do you have any other recommended part?
Thanks,
Hiro