Other Parts Discussed in Thread: TL331, TLV3401, TLV1701
Hello TI,
Could help us to provide Schmitt trigger schematic for below condition? also, we need you suggestion small package comparetor, thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Use a Schmitt trigger calculator like https://daycounter.com/Calculators/Comparator-Hystereses-Calculator.phtml or http://www.aaabbb.de/NonInvertingSchmittTrigger/NonInvertingSchmittTrigger_en.php.
To make the output switch between 6 V and 7 V, use a voltage divider instead of a single pull-up resistor.
The TL331 is cheap and fast; the TLV3401 uses little power; the TLV1701 is available in packages smaller than SOT-23.