Hi.
I'm testing INA226EVM.
Shunt resistor is 8.2ohm.
because 81.92mV / 10mA = 8.192ohm
When I connected 100 kilo ohm for load, INA226's current displayed 39.34uA and ampere meter is 33.2uA.
What's my fault?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I'm testing INA226EVM.
Shunt resistor is 8.2ohm.
because 81.92mV / 10mA = 8.192ohm
When I connected 100 kilo ohm for load, INA226's current displayed 39.34uA and ampere meter is 33.2uA.
What's my fault?
Thank you for reply.
What is the input bias current of INA226?
I think low-side measurement.
Currency is about 400mA through shunt resistor(8.2ohm).
I = 3.3V / 8.2 = 0.4024
Calibration registor value is attached file.
I got it.
Input bias current of my INA226EVM is 3.07uA.
Does the input bias current vary each INA226?
When mass production process, how does input bias current measure?