Hi,
The LMH6642 is stated to be short circuit protected for Vs < 6V at room temp and below. My application will see industrial temps (Up to +85 C ambient) and I need to know if I will need to design in further protection. Is there information available about short circuit protection for temperatures above room temp? If not, cold this be determined using maximum allowable power dissipation?
Thank you and best regards.
Edit: Maximum expected sourced voltage is 10V peak to peak.