This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM319: LM319

Part Number: LM319


What is the proper pinout for the LM319 14 pin pdip? The spec sheet I have has discrepancies.  rev jan 2016

Thanks

  • Hello Fritz,

    If you are referring to the "Pin Functions" description table on page 3, it is (very) incorrect. I will have to get that fixed.

    The 14 and 10 pin pinout images are correct. I verified them against an old National datasheet.

    Correct 14 pin pinout:

  • Since we haven't seen any additional questions, I am assuming that the answers have addressed your question and will be closing this thread. If any additional questions come up, feel free to reply to reopen or to create a new post.
    Chuck