Part Number: XTR111
Hi,
i would like to know what's the maximum current boost using the schematic in the XTR111 datasheet.
At first i thought that it was limited just by the transistor gain and 5mA base, but i tested a 50mA power consuption with a MMBT3904 and the XTR111 burnt.
Now i'd like the confirmation that if it's ok to work with this current (the goal is 200mA), to make more tests.
Thanks