This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC6042: LMC6042 Power Supply Current Exceeds Specifications

Part Number: LMC6042
Other Parts Discussed in Thread: LM5165

We are using this Ultra Lower Power Opamp as Dual Noninverting Amplifier and in 4-20ma 2 wire Circuit.

The Power Consumption of SOIC -8 Pin Package as per Specs is as per data sheets 

Measured Current for 5 Boards IS 7ma which is way beyond specifications, Can we get a resolution to this -please ??

ATTACHED SCHEMATICS 

Electrical Characteristics (continued)
Unless otherwise specified, all limits ensured for TA = TJ = 25°C. Boldface limits apply at the temperature extremes. V+ = 5V,
V− = 0V, VCM = 1.5V, VO = V+/2 and RL > 1M unless otherwise specified.
Typical(1) LMC6042AI LMC6042I Units
Symbol Parameter Conditions Limit(2) Limit(2) (Limit)
IS Supply Current Both Amplifiers 20 34 45 μA
VO = 1.5V 39 50 Max
Both Amplifiers 26 44 56 μA
V+ = 15V 51 65uAMax