Hi Team,
I received an inquiry from my customer on the AMC1200B. What will be the Output Voltage on VOUTP and VOUTN if only VDD2 is present (3.3V).VDD1 is Zero volts. Assuming the differential voltage on the inputs VINP and VINN can vary from 0 to 250mV.
Also please consider two cases below:
- VDD1 always zero but VDD2 has proper bias and there are input signals on VINP and VINN
- VDD1 and VDD2 initially have good steady-state bias, then VDD1 is removed while the VINP and VINN signals are present
We are interested to know what kind of VOUTP and VOUTN signals we will see – what levels and if these are consistent or bound what voltage level. This way, the DSP receiving the VOUTP and VOUTN signals can manipulate this and/or ignore if there is no valid input-side bias
Thanks!
Best Regards,
Alfred