Other Parts Discussed in Thread: LM324, DRV8800
I am using a 40 Khz square wave from a micro controller to my ultrasonic transmitter to measure distance from the receiver. However, I needed to increase the range of my system from my present value of approx. 1.5 m. For that, I was trying to amplify the 3.6 V ( with 0V baseline) square wave given to the transmitter. I tried using first, a LM324 amplifier circuit and then another NPN transistor amplifier circuit, but in vain. Could anyone suggest some circuit for the same as I was not an expert in electronics, so was finding it hard to do so?