Part Number: ISO224
Hi forum,
I cannot find any statement about the IMRR (isolation mode rejection ratio) in the datasheet of the ISO224.
Can anybody help me to find this parameter?
Rolf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO224
Hi forum,
I cannot find any statement about the IMRR (isolation mode rejection ratio) in the datasheet of the ISO224.
Can anybody help me to find this parameter?
Rolf
Hi Tom,
thank you, 140dB sounds great.
For me an analog isolation amplifier is mainly used for an isolated measurement of (shunt-) voltages.
In this respect the IMRR vs. frequency should be of greatest concern.
I wonder that this parameter is lacking in so many datasheets.
CMTI is certainly interesting but I find IMRR vs frequency more useful.
Regards
Rolf
Hi Rolf,
Thank you for the input! I'll see if we can get the IMRR data into future datasheets.