Other Parts Discussed in Thread: INA138, INA139, INA169, INA168, DRV425, AMC1300, INA190
Dear all expert :
Do we have AC OP which can detect current ?
the spec like this : AC90V~125V
Current 15A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Dustin,
Thanks for considering to use Texas Instruments. What is the minimum current level you need to measure and what is the frequency of your AC signal? You might be able to use the INA138, INA139, INA168, or INA169 in the implementation described here. Alternatively, you might consider using the DRV425 such as described in this technote. Lastly, you may want to consider some isolation amplifiers like the AMC1300, which can be found here.