Part Number: LMV358
Other Parts Discussed in Thread: LMV324-N, TLV342
Hello,
I want to use LMV358 in follower voltage to drive LED. I put the LED directly with a serie resistor to the output of the AOP and I change the input voltage at Vin+ pin.
I have a supply voltage of + 5Vdc.
My question is what is the maximum output current. I see in the datasheet P6, is 60 mA max is sourcing or 160 mA in sinking. In which case I am ?
Best regards