I built microcontroller based( arduino nano) solar battery charger unit. I added the schematic. I set up the circuit and try it with adjustable power supply instead of solar panel for input. I read voltages and output current correctly ( but output current value need calibration ) , but I cannot correctly read input current. While I am changing the input voltages ( current on power supply screen changes ), INA213 of input is always same value ( like 2110 mA ) and never changes. I tried it on many different pcb boards but it is same. What should I do? Is INA213 eaisly broken down?
Could you help me ?
( I choose shunt resistor as R040 ( 40m ohm) ( arduino is 5V and current range 0.01-2A => (5/50)/2 = 50 mohm so I choose R040 . Is there a mistake of calculating and choosing shunt resistor) )
And I want to learnd accuracy of INA213 in that condition?
Best Regards