Part Number: LMV331
Hi Team,
Please help to confirm the thermal data of LMV331IDBVRG4, which is not list on data sheet.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Daniel,
FYI: It looks like the LMV331IDBVRG4 will soon be obsolete.
The "G4" suffix denotes a "green" (non-Pb) package back from when the packages still contained lead.
Current devices have been converted to "green" packaging, so you do not need to order the "G4" version. The "G4" versions are obsoleted as the packages are converted.
So you should order the LMV331IDBVR instead, which is essentially the same device (same die, same package).
Hello Daniel,
The results are in:
|
Device Name: |
LMV331IDBVR |
|
Result- Theta JA-High K (standard datasheet value): |
232.8 |
|
Result-Theta JC, top (standard datasheet value): |
149.4 |
|
Result-Theta JB (standard datasheet value): |
89.7 |
|
Result- Psi JT (standard datasheet value): |
61.5 |
|
Result- Psi JB (standard datasheet value): |
89.2 |
|
Result-Theta JC, bottom (standard datasheet value): |
n/a |
Note: These new numbers are based on thermal modeling and should be more accurate than the old template-based numbers currently in the datasheet.