Part Number: THS4521
Dear Expert
Thank you for your special support.
My customers are considering THS4521.
They have the following questions.
■situation
-VS + = 5 V, VS- = 0 V
-Vocm = 1.5 V
-single-ended input,
-gain 1 time
■how to use
For input ± 1 V, Vout + and Vout - output each output 1 V to 2 V.
(Vout+ = 1V, Vout -= 2 V at -1 V input, Vout + = 2 V, Vout - = 1 V at + 1 V input)
■question
Datasheet From the graph of Figure 31,
we believe that there is no problem with how customers use it.
Please let me know if you can use it.