Part Number: LOG114
Other Parts Discussed in Thread: LOG112,
I want to use the LOG114 to measure photo current over the range 1nA to 100uA (5 decades). I plan to drive I2 with a 3.16uA reference current. I know the LOG112 has better DC accuracy, but it is too slow for this application.
I would like to compensate (in firmware) for offset and perhaps gain error. What is the best way to determine amplifier offset voltage? At first I thought I could leave I1 open and read the output, but I don't know if the LOG114 will behave properly with I1 = 0. I plan to use a precise external 2.5V Vref source to generate 3.16uA Iref. Could I drive both inputs with 3.16uA and read the output? Will that reading be a good number to subtract from actual readings to account for offset? Is there a better way?
Thanks,
Richard