This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91200: Replacement amp for LMP91200

Part Number: LMP91200
Other Parts Discussed in Thread: LMC6492, LMC6062, LMP7716, LMP7712, LMC6482

My company currently makes a pH meter using the LMP91200, and it works very well.  As part of a lifecycle management exercise, I am redesigning a the circuit to use a traditional dual op-amp rather than the LMP91200.  I don't need the VREF divider, and I will feed the VCM buffer (as a follower) with a 512mV reference voltage at the non-inverting terminal.  I know the pH buffer needs to have an extremely low input bias current due to the ultra low current (fA-pA) coming from the probe INP.  Ideally, I'd like to use a dual OpAmp for convenience.  I was considering the following: LMC6082, LMC6492, LMP2232, and LMC6482.  Are these appropriate and am I missing anything?