Part Number: INA169
Hi Team,
cusotmer would like to seek the similiar function as INA169 with EVM. (sense current and transfer to voltage). could you please recommend the proper or new on for this application?
Another question for INA169 max output voltage.
If cusotmer would like to monitor 12V/5A(max), the pin5 Vdd is 5V, the Vout max is limit to 5-0.7-(Vin+-Vin-).
If the Vout reach the limit, the Vout will keep at the Vout max level and won't trigger any protection by IN169 itself, right?
BR,
SHH