Other Parts Discussed in Thread: ADS1259, PGA281
Hi I am an intern experimenting on the PGA281EVM to amplify a signal.
I am new to the board, so i followed the circuit diagram from SBOS664A less the ADS1259 ADC.
The current setup I am using is
VSP: +15V
GND: 0V
VSN: -15V
VDD: +3V
VSOP:+5V
VSON: 0V
I am using external sources for the power supplies.
I have tested the gain using test input signals of 1Khz 200mVpp Sine Wave with 180 Degrees Phase Deviation.
The following are my observations
1) If I turn on all the power supply, for the VSOP to reach 5V, i need to set the current to 130mA. But then the differential output will not have any signals.
I have then lowered the current to 100mA, the V will be 4V, then i will be able to have an output.
The Range for VSOP is (+2.7V ~ 5.5V), so I am puzzled why it is operating @ 4V.
2)The output signal starts to be stagnant after a certain value of gain, causing the differential output to be different from the expected output.
May I know what would be the reason to cause this problem?
|
Differential Input |
G3:G0 |
G4=0 |
Expected Output |
Differential Output with VSOP @ 4V,100mA |
|
400mVpp |
0000 |
0.125 |
50mVpp |
52mVpp |
|
400mVpp |
0001 |
0.25 |
100mVpp |
100mVpp |
|
400mVpp |
0010 |
0.5 |
200mVpp |
204mVpp |
|
400mVpp |
0011 |
1 |
400mVpp |
400mVpp |
|
400mVpp |
0100 |
2 |
800mVpp |
800mVpp |
|
400mVpp |
0101 |
4 |
1.6Vpp |
1.5Vpp |
|
400mVpp |
0110 |
8 |
3.2Vpp |
2.2Vpp |
|
400mVpp |
0111 |
16 |
6.4Vpp |
2.6Vpp |
|
400mVpp |
1000 |
32 |
12.8Vpp |
2.6Vpp |
|
400mVpp |
1001 |
64 |
25.6Vpp |
2.6Vpp |
|
400mVpp |
1010 |
128 |
51.2Vpp |
2.6Vpp |
|
|
1011 |
RESERVED |
|
|
|
|
1100 |
RESERVED |
|
|
|
|
1101 |
RESERVED |
|
|
|
|
1110 |
RESERVED |
|
|
|
|
1111 |
RESERVED |
|
|