This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM393: Schmitt trigger using LM393

Part Number: LM393
Other Parts Discussed in Thread: TLV1701

Hello all,

I need schmitt trigger using LM393 comparator which can use single supply of 5V.

Also upper trip point is 1V and lower trip point is 0.45V.

Please anyone could design schimtt trigger for the above specification

Thank you