Part Number: TLV8541
Other Parts Discussed in Thread: LMP91002
I have an application with a gas sensor that has an output of about 5nA/ppm, and I want to be able to accurately detect very low concentrations (e.g. 1ppm) as well as high concentrations (e.g. 500ppm). Cost and power (battery application) are critical; we really can't afford more than about 10uA continuous draw, and cost is important so using a more integrated part like the LMP91002 is problematic.
I'd like to use this part with a very large feedback resistor (maybe 39Mohm) for the low ppm case and a smaller resistor (maybe 680k) in parallel with a FET to disable it for the wider range. Then the MCU that reads the output of the TIA could decide when to switch between them.
My question is, is it practical to use a 39M feedback resistor with this part, and expect accurate readings?