This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5056A: Pd(Power dissipation)

Part Number: LM5056A

Dear Team,

How to calculate this device's maximum Pd(Power dissipation)?

BR

Kevin

  • Hi Kevin,

    Based on the datasheet, the power dissipation would consist that of two supplies, the analog and the digital. Therefore the total would be 48V*1.4mA + 5V*6.8mA, assuming the setup is identical to the spec table.

    Regards, Guang

  • Hello Kevin,

    It's been over two weeks since your last post, so it seems like your issue has been resolved. I will close the thread for now, but if you have any further questions you can reply to re-open it or start a new thread with a new question.

    Best regards,

    Ian Williams
    Applications Manager
    Current & Magnetic Sensing