Part Number: INA199
Other Parts Discussed in Thread: TPS568215
Hi guys
Our customer is using our INA199 as server PSU output current sense. Common mode voltage is 12V. and the power supply is 16V-GND and REF is tied to GND. But we found an issue about INA199 input:
schematic:
The output current sense circuit is like above. Every time we power on, we can control the TPS568215 EN Pin is low(which means disable the buck output, so the output should be GND). But we found the output will be 2V. It is not be GND(0V).
Firstly, we thought it is related to the buck device. But we test the SW pin of the TPS568215. We found the SW have no any signal(PWM).
Secondly, We removed the inductor L104. So the Buck device will separated to the output circuit. But we found the output voltage(INA199 IN+) will still be 2V. Here I don't know what lead to the INA199 INPUT common mode voltage 2V. There is no any other connections except the buck device and the INA199.
Thirdly, we removed the R680 and R687, the output voltage will be GND.
Do you have any recommendation about this issue?
Any feedback will be appreciated.
Thanks
-Pengfei