Part Number: OPA855
Hi,
Is it possible to get an OPA855 with the SOCI08 package or any other package instead of WSON to be easieable to solder it.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bob,
it's really hard to handle a decompensated 8GHz GBP OPAmp! That's a totally different story than to work with a normal HF OPAmp. Even sub millimeter signal lengths play a role. Because of this it would be really hard (read impossible) to make a OPA855 circuit work, if the OPA855 would come in a SO8 package.
A WSON package should be mounted with machine soldering. For prototyping I use hot-air soldering in combination with pre-heating. See also here:
https://e2e.ti.com/support/amplifiers/f/14/p/701057/2618501#2618501
Kai