This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA114: issue with different grounds

Part Number: INA114


Hi,

I have a bridge diff. signal and I want amplifier this signal with a Instrumentation Amplifier.

For that I use the INA 114.

the amplifier signal should be convert with a SAR ADC. The SAR ADC use a 3.3V power supply. The analog input pin is the P2_7. the corresponding AGround Pin 1 on conector J1. When I connect the following schematic the converted value is the Ref voltage. for that I thing there is a ground issue.

enclosed the schematic and the measured value.

many thanks you your support.

Carsten