This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: A question about INA240 output capacitive load

Part Number: INA240

Hello,

We are using INA240A2 to measure motor current.  However, per the datasheet, the INA240A2 output maximum capacitive load should be limited to 1nF.  So, we added a buffer in front of a 20Hz low-frequency filter.  My question is to find out if it is necessary to have the buffer in front of the filter to limit the capacitive load even though a resistor is located at the output.  I've attached the schematic for your reference.  I would appreciate it if you could respond to me promptly.

Best regards,Attachment.docx