Part Number: PGA309
Other Parts Discussed in Thread: XTR117,
Hello,
We are designing a sensor board for conductivity measurement using Wheatstone's Bridge. We plan to use PGA309 and XTR117 for converting voltage to current loop.
We found one application note (slau526- Digitally Calibrated Bridge Sensor Signal Conditioner with 4mA to 20mA Current Loop Output) which we are referring.
Following are my queries:-
1) How does the EEPROM (interfaced with PGA309) store calibration settings? How to write/ read into the EEPROM? There is no Microcontroller on this board.
2) The circuit diagram in slau526 (page 27) show PRG pin of the PGA309 is connected to 1W. and further the 1W is brought on JUMPER. can you please provide more details as to why this provision is made and whether is it mandatory to connect it the way it is connected or we can leave it open (or connect to VOUT as suggested in some TI documents).
Thanks in advance.
Ankeet Gugale.