This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As per the datasheet recommendation we are planning to use Supply voltage (VS) as 5V (VS+ = 2.5 V, VS– = –2.5 V).
we are planning to use amplifier LMH5401 as ADC driver and single ended 50-Ohm input to 200Ohm differential output.
For maximum Input voltage range at (VS & VS+) is mentioned as (VS–) – 0.7 and (VS+) + 0.7. So we can take it as VS+ = 3.3 V, VS– = –3.3 V as absolute maximum input levels.
Now we have assumed our input is 50Ohm matched (single ended) and for maximum of +/3.3V (6.6Vp-p) if we calculate for 50 Ohm load the input power will be +20.4dBm.
Can we take +20.4dBm as absolute maximum RF input power when we use Supply voltage (VS) as 5V (VS+ = 2.5 V, VS– = –2.5 V)? Is it our above calculations are correct?