This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7347: Could THS7347 use for 1080p and WUXGA?

Part Number: THS7347

Customer was using THS7347 as the mux for VGA1 and VGA2, without any issues for the resolution XGA and WXGA. 

They plan to use THS7347 as the mux for 1080p and WUXGA in the future. 

They want to know (1) if THS7347 is capable? and (2) Is their any design points necessary to be changed? 

pixel frequency
XGA(1024x768/60Hz)  =65MHz
WXGA(1280x800/60Hz) =83.46MHz
1080P(1920x1080/60Hz) =148.5MHz
WUXGA[1920x12000/60Hz (RB)] =152MHz