Part Number: THS4551
Dear all,
Currently I am designing a single ended to differential front end for an IEPE microphone. The microphone is AC coupled into the front end and amplified/converted using the THS4551 to a differential signal driving a cirrus logic ADC.
In the datasheet of the THS4551 in the section design rules it is stated that the ground/power plane should be opened up around the input and output pins to reduce/prevent parasitic capacitance. Does this mean opening up the top layer ground fill or also the ground and power plane below the THS4551? (For information, my stack up is <Signal top with ground fill> - <GND> - <Power> - <Signal bottom with ground fill>. The THS4551 is on the top layer.)
BR,
Carsten Voort