Other Parts Discussed in Thread: NE555, TLV3701, LM555
Dear *,
i have a pressure sensor that has an output from 0-5V depending on the pressure.
I want to make a circuit when the pressure drops below a level that the circuit generates a square pulse with defined pulse duration.
I want to do it without a uC.
My idea is to use a compactor IC and a timer IC ( NE555) and a reference voltage IC.
Please can you suggest the Compactor, timer and reference IC for this application ( please note that i need all the ic to be in DIP package)
Best Regards,
D.