Part Number: LM239
Good morning, I am using LM239 and I want to supply it with 11V whereas my output pull-up voltage is 35V tied to 15k pull-up resistors. Which is the maximum output voltage of LM239 when supplied with 11V?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM239
Good morning, I am using LM239 and I want to supply it with 11V whereas my output pull-up voltage is 35V tied to 15k pull-up resistors. Which is the maximum output voltage of LM239 when supplied with 11V?
Thank you!
Thank you for the reply.. I have another question.. What about the input common mode range of the comparator.. It is valid what the datasheet says about out of range at page 13?:
The following list describes the outcomes of some input voltage situations.
• When both IN– and IN+ are both within the common-mode range:
– If IN– is higher than IN+ and the offset voltage, the output is low and the output transistor is sinking
current
– If IN– is lower than IN+ and the offset voltage, the output is high impedance and the output transistor is
not conducting
• When IN– is higher than common mode and IN+ is within common mode, the output is low and the output
transistor is sinking current
• When IN+ is higher than common mode and IN– is within common mode, the output is high impedance and
the output transistor is not conducting
• When IN– and IN+ are both higher than common mode, the output is low and the output transistor is sinking
current
Thank you..