Part Number: TLC2272
Other Parts Discussed in Thread: , LM7705
Hi Sir/Mam,
Greetings!!!
We are facing some difficulties in understanding of the U7A output configuration.The output of U7A is depends on D5 and R49.
We tested some cases as mentioned below :
| TP29 | TP21 | U7A Pin #2 | U7B Pin #7 |
| 10mV | 149mV | 47.4mV | 198mV |
| 20mV | 155mV | 50.2mV | 204mV |
| 30mV | 161mV | 53.6mV | 212mV |
| 40mV | 168mV | 57.6mV |
223mV |
We already gone through the datasheet of TLC2272,But we can't find the input output relation.
Please guide us in this.
Kindly let me know if you require more information.