Part Number: LMP2022
We have a situation where the supply voltage, normally +5V nominal, is off (assume 0V) and the V- pin is connected to ground. There is a series resistance of 14Kohms connected to pin 6 (minus input). There is an input connected to that series resistor that can independently sustain a voltage of -3.9V. My questions are as follows:
- Can this induce circuit overstress for input pin 6?
- If conduction occurs, how much current can be anticipated coming from pin 6?
I would appreciate assistance on this issue. Thank you.