Other Parts Discussed in Thread: LMH5401, OPA855, OPA859, THS3217, THS4304
Hello,
i'm using a LMH5401 to amplify (x10) a differential signal. The Vcm of the input voltage is around 3V. The LMH5401 is powered with a 5V single supply and Vcm is set at 2.5V.
This works fine. I want to convert the output differential signals of the LMH5401 to a single ended signal centered around 0V (excursion +-1V ~ +-2V around 0V).
I was looking for a op-amp with GHz bandwith, powerable in +-5V and working in voltage-feedback mode to use it in a simple voltage subtractor mode.
I failed to found the right op-amp. Did I missed something or am trying to do it in the wrong way?
Thank you,
Best regards