This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1300: AMC1300 single - end input mode, use problem

Part Number: AMC1300

Holle:

We are pushing AMC1300 to replace avgo_acpl-c790. Our competitor (acpl-c790) supports two working modes of differential input and single-end input. In the AMC1300 datasheet, there is only differential input working mode.

If the AMC1300 is also connected to a single end connection, I wonder if there is any performance impact?

Best Regards

Leon