Other Parts Discussed in Thread: VCA824, THS3217
Hi,
I have two sinusoidal inputs at frequencies from 15MHz to 50 MHz with an amplitude of approx 1.4Vpp. I need to accurately measure the difference in amplitude between them (approx 0.1% to 1%) but I am having issues to find a device which fulfill the requirements.
I guess the main issue is the CMRR at these frequencies, so an off-the-shelf INA or Difference amplifier would not be good enough for this particular application...
Any ideas on how to implement this?
Thanks a million,
Kind regards,