Other Parts Discussed in Thread: TLV3701-Q1, OPA171-Q1, , TLV3701, TLV3702, TLV2464, SN74LVC1G66-Q1, TS5A3159
I use TLV3701-EP to convert open-gnd connection to 5V logic level. I have 4 of these comparator circuits on the card, and after several hours (3-6 hours) one of the comparators burn, and then circuit continuous to work well once I replace the burnt TLV3701-EP with another TLV3701-EP, until another one burns. I try to figure out why. Supply is single 5V, inputs never exceed 5V. So overvoltage should not be an issue. All two input pins and output pin are connected to rest of the circuitry with series resistances in the order of tens of kohms in between, so I don't think overcurrent is an issue. I measured the 5V supply and it is clean.I thought powering sequence might be the problem, because one of the inputs might being pulled up to around 4.5V at power up before 5V supply rises, but datasheet claims that VCC+5 volt is acceptable at inputs. Also this pull-up operation is done with a 560kohm resistance, so TLV3701-EP should be able to clamp overvoltage even if it occurs, because input current limit is 10mA. So I don't think powering sequence is an issue. Then I thought maybe ESD is the problem, because there is not any information in datasheet of TLV3701-EP. But then I realize TLV3701-Q1 datasheet includes information about ESD protection. I assume TLV3701-EP and TLV3701-Q1 have the same structure and TLV3701-EP datasheet does not include ESD information because it is old (please correct me if I am wrong). So I dont think that ESD is the issue either.Then I replaced four TLV3701-EP's on the board with OPA171-Q1 and tested, circuit worked without any fault for 24 hours (I know that using an opamp as comparator is not a good practise). I am trying to find why TLV3701-EP comparators which are initially fine burn after several hours, any help is appreciated.