Hi team,
When my customer use the DRV595 and they find some spurs related to the oscillator spur.
Below is the schematic
issue 1: They use the 4.7k resistor to pull up the FAULZ pin to 3.3V, but the voltage keep as 1.3V when they power up the device. Can you help to review the schematic and find the possible cause?
issue2: When they increase the voltage of the between the VIN+ and VIN-, they find some spur that in VIN+ and VIN- , and also FAULTZ pin.
Keep the VIN+ as 3V and decrease the VIN- to 2V,
- There show some spurs in IN+ and IN- and the FAULTZ. The spur of FAULTZ also cause the FAULTZ switch to low voltage.
- The spur frequency is 500kHz which is the same frequency of the oscillator frequency setting by the FS0-2.
- When the voltage between IN+ and IN- increase, the level of the spur increase.
Please help to analyze the finding and find the possible cause.
Lacey
Thanks a lot!