This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240-Q1: Part No difference

Part Number: INA240-Q1

Dear TI team:

    What's the difference between INA240A1EDRQ1 and INA240A1QDRQ1?

    Thanks!

Regards!

Eric

  • Hi Eric,

    Both E and Q versions are built with the same die and they both go through exactly the same final test. The only tangible difference between the two is bond wire material – E uses a higher purity 99.99% gold wire; while Q uses a 99% gold wire.

    Regards, Guang