Other Parts Discussed in Thread: OPA2196, OPA2197, OPA333, LMC6061, OPA241
I need an alternative for the above mentioned part . i find an alternative from TI OPA2197/ OPA2196, but it has higher Iq current . need other suggestions
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rejo,
If the maximum supply voltage in the application is +5 V, then a precision op amp such as the OPA333 should be a suitable replacement for the MAX478C/LT2178.

If the supply is +4.5 to +15 V, the higher supply voltage LMC6061 might be an option:

However, if the supply voltage requirements are even higher, such as +/-12 or +/-15 V, the OPA241 might be an option:

These device selections where based on the low operating current requirement. However, we would really need to know what parameters are most important in your application to help select the most suitable op amp.
Regards, Thomas
Precision Amplifiers Applications Engineering