Part Number: INA226EVM
Other Parts Discussed in Thread: INA226
I have just started to use the INA226EVM and I am little confused about how to set the Configuration Register.
I have a
Shunt Resistor = 0.0025 Ohm
BUS voltage = 4.84
Shunt Voltage = 1.978mV
Doesn't this mean that the EVM should be calculating an approx. Current = 79.12mA ?
I have set the configuration Method : Current LSB
Set Max Current : 500mA (this is what I would expect when I start to transmit on my device - currently it is at standby)
However the EVM tells me that the low LSB :15.26uA & High LSb:122.1uA. When I set Current LSB to 15.26uA so the current = 192mA ? Which is much higher than what I expected ? It is only when I set the Current LSb = 6.5uA that I get my expected current approx. 80mA - ??
When I set the Max Current to 100mA so the range of Low LSB: 3.052uA High LSB:24.41 - that put my choice of 6.5uA within the range but What am I meant to do when I start to draw higher currents? Am I doing something wrong and how accurate are these current recordings going to be ?
I tried to read the data sheet of the INA226 regarding Programming Calibration Register value - but I am still confused ?
Please could someone please explain this a little ?