Part Number: OPA547EVM
Other Parts Discussed in Thread: OPA547
Dear TI engineers
I would like to use the improved Howland circuit using the OPA547EVM PCB. my purpose is to drive a MEMS resistor of a few ohms typically from 10 to up to 500 ohm or even 1k with an AC current. as an input i want to use a voltage function generator at low frequency less than 30Hz. Do you think the OPA547EVM is fit for that purpose and is it plug and play or do i have to solder different components. i was thinking of making the circuit but if the TI PCB is fit i ll just buy it. awaiting your feedbkack.
Thanks for your inputs
Ahmed