Part Number: OPA357
Other Parts Discussed in Thread: TINA-TI, OPA837, OPA1678, OPA2189
Hello,
I'm trying to replicate Åckerberg-Mossberg Filter using OPA357. With the SNAA287A as reference, how can I get 400kHz center frequency?
The selected values are:
R4=R5=R3=R6=4.3K
C2=C3=91pF
C1=1nF
R1=6.8K
R2=66K
Rout1=1.5K
Rout2=8.2K
Cout1=2.7nF
Rc=2K
I'm not sure I got all values right. Any comments/suggestions?
Thanks!