Part Number: OPA858
Other Parts Discussed in Thread: ADS4225, LMH6518, BUF602, OPA820, OPA656
Hi,
Paralleling opamps will decrease noise and will therefore prevent degradation of SNR. But, what is the right way to do it?
I mean, just paralleling pin by pin is one possible way but then i will have to think about the input offset voltage and the feedback and gain resistors.
Would it be a right approach to just use one feedback resistor and one gain resistor for a set of say 4 opamps? I read somewhere that the offset would then be the mean value of all opamps. Is that correct?
The way i see it, it would be more convenient if i just parallelized pin by pin all opamps and then use one Rf and one Rg. What about the decoupling caps? Would i have to use the same number of caps just like in a case of one opamp? Since decoupling caps must be extremely close to the pins there is no way to use one set of de-caps for 4 opamps unless i find a way to place them one on top of the other and so on. Still, it doesn't sound right. One negative off course is the fact that the quiescent current will be multiplied by the number of opamps that will be used and given 20mA for the OPA858 the total for 4 opamps will be 80mA.
I am thinking about using 4 OPA858 in parallel followed by a LMH6518 which will directly drive an ADS4225 through a low pass.
Could you pls comment on my thoughts regarding the paralleling of multiple OPA858?
Thanks in advance
Regards
Manos